This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900适用灵敏度范围是否支持0.5mV/V?

Other Parts Discussed in Thread: PGA900, PGA300

PGA900手册描述其适用传感器灵敏度范围是1-135mV/V,请问能支持0.5mV/V的灵敏度吗?

  • 没在可支持的范围之内,应该是不支持的。

  •  该器件的最大激励电压是2.5V,输出电流也会限制在1.5mA以内。按照灵敏度为0.5mV/V来计算,最大输出电压只有1.25mV左右,内部最大增益为400V/V。考虑到内部有24Bit性能优异的ADC,采样一定是可以识别出信号变化。

    问题在于到底能用还不能用,取决于你处对系统精度的要求?比如0.5%还是更高要求。

    当然处理此类微小信号,电路设计上需要更多需要注意的地方。

  • 谢谢你的解答!如果我使用外部输出为10V的电压供电,这样应该能识别变化,但是我这里系统精度要求是0.1%,考虑到电源芯片的影响,电路设计时需要考虑哪些因素?

  • 你处所要设计产品的输出信号是模拟量(电压或者4-20mA)?如果是的话,可以考虑PGA300,使用更为简单,不需要代码开发。

    若用电压10V给前端芯体做激励,显然输出不能直接给PGA900/300输入。

    你处提到的0.1%精度指标是指综合精度要求吧,这样的话应该需要温度补偿和非线型补偿,PGA300/309应该很适合你处需求。

     

  •  谢谢!

    你上面说若用10V供电,信号无法直接送入PGA900,为什么?我在数据表中并未看到相关说明,还请帮忙。

  • 如果采用10V激励电压给芯体,则对应的共模电压远超出PGA900所能接受范围。当然,要是将10V直接给PGA900供电(VDD),因为改器件接受较宽范围供电这样是可以的。