Other Parts Discussed in Thread: PGA900, PGA300
PGA900手册描述其适用传感器灵敏度范围是1-135mV/V,请问能支持0.5mV/V的灵敏度吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
该器件的最大激励电压是2.5V,输出电流也会限制在1.5mA以内。按照灵敏度为0.5mV/V来计算,最大输出电压只有1.25mV左右,内部最大增益为400V/V。考虑到内部有24Bit性能优异的ADC,采样一定是可以识别出信号变化。
问题在于到底能用还不能用,取决于你处对系统精度的要求?比如0.5%还是更高要求。
当然处理此类微小信号,电路设计上需要更多需要注意的地方。
你处所要设计产品的输出信号是模拟量(电压或者4-20mA)?如果是的话,可以考虑PGA300,使用更为简单,不需要代码开发。
若用电压10V给前端芯体做激励,显然输出不能直接给PGA900/300输入。
你处提到的0.1%精度指标是指综合精度要求吧,这样的话应该需要温度补偿和非线型补偿,PGA300/309应该很适合你处需求。
如果采用10V激励电压给芯体,则对应的共模电压远超出PGA900所能接受范围。当然,要是将10V直接给PGA900供电(VDD),因为改器件接受较宽范围供电这样是可以的。