Other Parts Discussed in Thread: ADS8638
ADS8638根据手册上看写寄存器的时候,DOUT应该是0x0000的,但是为什么我写寄存器的时候,同时有数据输出?
以下是我的代码
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File
#include "SciSetup.h"
#define LedReg (*((volatile Uint16 *)0x41FF))
Uint16 *ExRamStart = (Uint16 *)0x100000;
void senddata(Uint16 a, int num);
#define ALPD GpioDataRegs.GPADAT.bit.GPIO26
// Prototype statements for functions found within this file.
// interrupt void ISRTimer2(void);
void delay_loop(void);
void spi_xmit(Uint16 a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);
unsigned int Spi_TxReady(void);
unsigned int Spi_RxReady(void);
void main(void)
{
Uint16 sdata; // send data
Uint16 rdata; // received data
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Setup only the GP I/O only for SPI-A functionality
// This function is found in DSP2833x_Spi.c
InitXintf16Gpio(); //zq
InitSpiaGpio();
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0;
GpioCtrlRegs.GPAPUD.bit.GPIO26=0;
GpioCtrlRegs.GPADIR.bit.GPIO26 = 1;
EDIS;
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
spi_fifo_init(); // Initialize the Spi FIFO
spi_init(); // init SPI
// Step 5. User specific code:
// Interrupts are not used in this example.
LedReg = 0xFF;
ALPD=1; //PowerUP
// spi_xmit(0x080E);//PowerDown
// spi_xmit(0x0800);//PowerUp
for(;;)
{
// Transmit data
spi_xmit(0x0201);//自动采集
}
}
// Step 7. Insert all local Interrupt Service Routines (ISRs) and functions here:
void delay_loop()
{
long i;
for (i = 0; i < 1000000; i++) {}
}
void spi_init()
{
SpiaRegs.***.all =0x000F; // Reset on, falling edge, 16-bit char bits
SpiaRegs.***.all =0x0006; // Enable master mode, normal phase,
// enable talk, and SPI int disabled.
SpiaRegs.SPIBRR =0x00FF;
SpiaRegs.***.all =0x008F; // relinquish SPI from reset
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
}
void spi_xmit(Uint16 a)
{
Uint16 rdata1; // received data
if(Spi_TxReady() == 1)
{
SpiaRegs.SPITXBUF=a;
}
while(Spi_TxReady() != 1)
{
}
if(Spi_RxReady() == 1)
{
rdata1 = SpiaRegs.SPIRXBUF;
}
delay_loop();
}
void spi_fifo_init()
{
// Initialize SPI FIFO registers
SpiaRegs.SPIFFTX.all=0xA040;
SpiaRegs.SPIFFRX.all=0x204f;
SpiaRegs.SPIFFCT.all=0x0;
}
unsigned int Spi_TxReady(void) //发送就绪
{
unsigned int i = 0;
if(SpiaRegs.SPISTS.bit.BUFFULL_FLAG == 1)
{
i = 0;
}
else
{
i = 1;
}
return (i);
}
unsigned int Spi_RxReady(void) //接收就绪
{
unsigned int i = 0;
if(SpiaRegs.SPISTS.bit.INT_FLAG == 1)
{
i = 0;
}
else
{
i = 1;
}
return (i);
}
//===========================================================================
// No more.
//===========================================================================