This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助求助:ads1675高速ADC输出结果异常

Other Parts Discussed in Thread: ADS1675

ADS1675模数转换器输出结果异常。配置的参数为转换速率500K,参考电压3V,差分输入共模电压2.5V,SCLK使用内部时钟,COMS接口,模拟电源5V,数字电源3.3V,晶振32Mhz。

测试各管脚电压与配置均无错误,SCLK和DRDY也与配置的参数一致。

以下是遇到的问题:

1  差分输入为0V时,输出结果为一数值很大的值。

2  差分输入为2.5V时,输出结果仍为很大的值,与输入0V时值不同。

3 输入变化,输出也变化,但是转换结果不正确。

4 芯片有发烫现象出现。