This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3082通讯问题

Other Parts Discussed in Thread: ISO3082

HI 你好,我使用你们公司的ISO3082和MAX3485E 通讯,发现3082出来的数据到AB是对 的,MAX3485E 反回来的数据AB到3082的管脚上是对的,但是转出来的串口数据总出问题,无论AB上的电阻怎么接 怎么改都是解决不了,请相关工程师答复下,谢谢!

  • 你的问题是不是可以理解为: ISO3082 txd 的传输信号正常, 但是 AB  到 RXD 信号不正常?

    不知道怎么个不正常?  那条数据收发控制信号怎么处理的呢?

  • ISO3082 是一款隔离的485收发器,MAX3485在ti官网上没找到,也是485收发器吧?如果是的话,可以使用一片ISO3082既带隔离,又是收发器,来替代收发器+隔离功能。

    能否把电路图发上来看下?

  • 是的,到RXD是不正常了。接受的信号出错。把3485换成你们的SN65HVD12IDRE这个料就收发正常了。感觉3082的兼容性不好。

  • MAX3485是美信的一款非隔离的,3082用的是我们板子上面的,通信的时候发现,对方收得到消息,也回复了(通过淘宝上面普通的485工具连接在3082,的AB端测到),但是3082转到UART的时候,信号就错误,我后来使用了,以前板子上用过的SN65HVD12IDRE这个料,把它替换3485。就是正常了。应该是TI这个料不兼容性差。

  • MAX3485是美信的一款非隔离的,3082用的是我们板子上面的,通信的时候发现,对方收得到消息,也回复了(通过淘宝上面普通的485工具连接在3082,的AB端测到),但是3082转到UART的时候,信号就错误,我后来使用了,以前板子上用过的SN65HVD12IDRE这个料,把它替换3485。就是正常了。应该是TI这个料不兼容性差。