Other Parts Discussed in Thread: ISO3082
HI 你好,我使用你们公司的ISO3082和MAX3485E 通讯,发现3082出来的数据到AB是对 的,MAX3485E 反回来的数据AB到3082的管脚上是对的,但是转出来的串口数据总出问题,无论AB上的电阻怎么接 怎么改都是解决不了,请相关工程师答复下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISO3082 是一款隔离的485收发器,MAX3485在ti官网上没找到,也是485收发器吧?如果是的话,可以使用一片ISO3082既带隔离,又是收发器,来替代收发器+隔离功能。
能否把电路图发上来看下?