This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP6678 + FPGA K7协同处理Rapid IO互联6678板卡

Other Parts Discussed in Thread: TMS320C6678

     TES600是北京青翼科技的一款基于FPGA与DSP协同处理架构的通用高性能实时信号处理平台,该平台采用1片TI的KeyStone系列多核浮点/定点DSP TMS320C6678作为主处理单元,采用1片Xilinx的Kintex-7系列FPGA XC7K325T作为协处理单元,具有1个FMC子卡接口,具有4路SFP+万兆光纤接口,处理节点之间通过高速串行总线进行互联。该系统通过搭配不同的FMC子卡,可广泛应用于软件无线电、雷达信号处理、基带信号处理、无线仿真平台、高速图形图像处理等应用场景。

技术指标

 FPGA + 多核DSP协同处理架构;

接口性能:

1. 1个FMC(HPC)接口; 

2.4路SFP+光纤接口; 

3.2个GbE千兆以太网口; 

4.2路外触发输入信号;

处理性能: 

1.DSP定点运算:40GMAC/Core*8=320GMAC; 

2.DSP浮点运算:20GFLOPs/Core*8=160GFLOPs;

存储性能:

1. DSP处理节点:4GByte DDR3-1333 SDRAM; 

2.DSP处理节点:4GByte Nand Flash;

3. FPGA处理节点:2GByte DDR3-1600 SDRAM;

互联性能: 

1.DSP与FPGA:SRIO x4@5Gbps/lane; 

2.FPGA与FMC接口:1路GTX x8@10Gbps/lane;

物理与电气特征 

1.板卡尺寸:171 x 204mm

2. 板卡供电:3A max@+12V(±5%)

3. 散热方式:自然风冷散热

 环境特征 

1.工作温度:-40°~﹢85°C,存储温度:-55°~﹢125°C;

2.工作湿度:5%~95%,非凝结

软件支持

1. 可选集成板级软件开发包(BSP):

2.DSP底层接口驱动;

3.FPGA底层接口驱动;

4.板级互联接口驱动;

5.基于SYS/BIOS的多核处理底层驱动;

6.可根据客户需求提供定制化算法与系统集成:

应用范围

1.软件无线电;

2.雷达信号处理;

3.高速图形处理;

x 出现错误。请重试或与管理员联系。