我的板子,当DRATE=2.5Hz PGA = 1时,不能稳定到16位。我的设置是将01H寄存器设置为0x88,将其均接到AINCOM上。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
在您的电路中采用的高精度基准源REF195, 如果是这样的话,输入电压需要大于5.2V以上,否则输出电压5V输出会偏离而造成严重的精度损失。输出电容也不需要100uF这么大,选用1~2.2uF陶瓷电容即可.ADC的AVDD.DVDD电容也推荐4.7~10uF陶瓷电容。
两外就是要注意数模隔离,各信号GND端点接GND Plane.