现在利用一个+15V和一个+3.3V供电,+15V经过一个117转+5V,让后将这个5V和3.3V分别作为164245的两个电源端实现5V到3.3V的电平转换。但是现在出现了我通电时间一长发现164245发出的声响,然后电流突变,一测发现5V和地短接了。请问这可能是什么原因导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在利用一个+15V和一个+3.3V供电,+15V经过一个117转+5V,让后将这个5V和3.3V分别作为164245的两个电源端实现5V到3.3V的电平转换。但是现在出现了我通电时间一长发现164245发出的声响,然后电流突变,一测发现5V和地短接了。请问这可能是什么原因导致的?
使用的是SN74LVC16245这款transceiver吗?这款的话,供电电压最大为3.6V,因此5V供电是不允许的,这是电源对地直接短路的原因吧。
您可以使用SN74LVC16T245这款,可以实现5V到3.3V的相互转换。 符合您的应用。
是的,您的理解是正确的,所有控制位,包括DIR,OE都是参考的VCCA,高电平的话只能接到VCCA。Xi Meng 说:wo g我刚刚测了一下取下的芯片,发现7脚的VCCB与地短接了。
另外请问一下方向控制位的高电平是不是只能VCCA供电,对于我这个来说就只能是3.3V供电提供高电平时,是吗?