我的研究需要DAC8820,我找到了DAC8820的评估板DAC8820EVM,所以可不可以推荐相应的控制板和控制软件,能够使我在电脑上连续输入数字信号,在评估板上输出模拟信号生成波形,?
如果没有的话,我可以使用FPGA控制评估板,实现我所需要的波形吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的研究需要DAC8820,我找到了DAC8820的评估板DAC8820EVM,所以可不可以推荐相应的控制板和控制软件,能够使我在电脑上连续输入数字信号,在评估板上输出模拟信号生成波形,?
如果没有的话,我可以使用FPGA控制评估板,实现我所需要的波形吗?
在EVM user's guide中有介绍和哪些主控兼容http://www.ti.com/lit/ug/slau190a/slau190a.pdf。
比如:
• Compatible with the 5-6K and HPA-MCU Interface Boards for use with a variety of Texas Instruments DSP Starter Kits (DSK) and micro controllers such as the TMS470
• Compatible with the TI Analog Interface Board from Avnet for use with Xilinx FPGAs
The DAC8806 and DAC8820 devices are 14-bit and 16-bit, multiplying DACs with a microprocessor and TMS320 DSP-compatible parallel interface.
Hi
• Compatible with the TI Analog Interface Board from Avnet for use with Xilinx FPGAs
这个没看明白,我还需要相应的TI接口板,才能用Xilinx 的FPGA控制DAC8820的评估板吗?
不可以直接连接控制吗?
这里的接口板应该指的是ADC-HSMC adapter card 和Xilinx FPGA 板子连接。
您参考下这篇手册,列举的是TI的ADC或DAC板子和xilinx FPGA接:
http://www.ti.com/lit/ml/slab058/slab058.pdf
可是文档上显示的DAC-FMC-Adapter 是用于高速DAC的,但是DAC8820不是高速DAC且文档中所列的也没有DAC8820.
因为我不是专门做硬件的,我的目的是使用做好的评估板实现我所需要的要求,主要是能够连续向DAC输入数据进而产生所需要的波形,然后我们已经有了xilinx的FPGA Virtex-5开发板,
我想问一下的是能不能用我们的FPGA板根据DAC8820的数据手册产生合适的时序控制DAC8820评估板?