This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DDC112的2个问题

Other Parts Discussed in Thread: DDC112

各位好!在使用DDC112对硅光二极管进行测试时

使用ARM芯片的时钟模块驱动DDC112,时钟模块之间的相位有严格的同步,使用ARM的SPI模块读取数据,一次读入5个字节,对应2组转换的数据。

问题1:

将输入端IN1接地,该组转换的结果显示为0(0x00000),而非手册中所说的4096(0x01000)。

问题2:

对DDC11的数字和模拟部分分别采用独立的线性电源供电(电源GND通过单点连接)时,出现如下现象:

1. 如果只上数字部分的5V电源,完全断开模拟部分电源,测量模拟部分电源输入显示约2~3V的固定值,且ref管脚显示相同的电压。由于ref电路此时可能未正常工作,所以可能是由于DDC112在ref端输出所致,请问是否正常。即在单单给数字部分供电时,是否存在电源部分耦合至模拟部分输入管脚的可能?

2. 如果先上数字部分的5V电源,再上模拟部分的5V电源,检测到数字部分电源输出电流过大,发热严重。而使用单电源供电时不存在此现象,此种情况是否正常?

谢谢

  • 对于这款来说,模拟电源和数字电源没有严格的上电顺序,在硬件这块,使用独立的线性电源或者同一款线性电源非别给AVDD和DVDD上电都可以,建议模拟电源和数字电源也是用磁珠连接即可。就像模拟地和数字地的处理一样。

    另外,上电时,在上电稳定之前不要给输入信号,datasheet中有描述:Prior to power-up, all digital and analog input pins must be LOW. At the time of power-up, these signal inputs can be biased to a voltage other than 0V, however, they should never exceed AVDD or DVDD.
  • 谢谢!我继续测试,有问题再和请教