采用TLV2553作为电压检测,当检测电压低于7V时,检测精度为±0.03V,当电压超过7V时,检测的精度会逐渐变大,并且采集到的电压值跳变比较严重。
比如采集采集16V时,采集到的电压在16.01~16.38V之间变化
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用TLV2553作为电压检测,当检测电压低于7V时,检测精度为±0.03V,当电压超过7V时,检测的精度会逐渐变大,并且采集到的电压值跳变比较严重。
比如采集采集16V时,采集到的电压在16.01~16.38V之间变化
我是通过一个100k和一个22k 精度为0.1%的精密电阻进行分压后,通过电压跟随器,然后进入TLV2553的。TLV的输入电压为0~3.3V之间,没有超过其VCC的电压。