This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2553 检测电压时,电压值越高,采集的精度越差,跳变比较大

Other Parts Discussed in Thread: TLV2553

采用TLV2553作为电压检测,当检测电压低于7V时,检测精度为±0.03V,当电压超过7V时,检测的精度会逐渐变大,并且采集到的电压值跳变比较严重。

比如采集采集16V时,采集到的电压在16.01~16.38V之间变化

  • 比如采集采集16V时?

    手册明确要求,输入信号不能超过 VCC 的。

  • 我是通过一个100k和一个22k 精度为0.1%的精密电阻进行分压后,通过电压跟随器,然后进入TLV2553的。TLV的输入电压为0~3.3V之间,没有超过其VCC的电压。

  • 您好,

    进入TLV2553的信号电压范围是0~3.3V之间,采集到的应该也在0~3.3V之间。“比如采集采集16V时,采集到的电压在16.01~16.38V之间变化”中的16.01~16.38V电压应该是您已经换算到分压之前的电压,那么换算之前精度怎样呢,换算之后精度不好可能与您的换算算法有关。
  • 您好,
    是这样的,当输入电压很低的时候,TLV2553的转换的数字量偏差很小,比如SPI读取的数字量为120时,偏差仅有±3的样子,当数字量变为3500时,其SPI读取的数字量偏差最大能达到±(40~50),不太明白为什么,SPI读取的数字量较小时,偏差比较小,SPI读取的数字量比较大时,偏差就比较大。
    另外,我想确认一下,TLV2553的采集精度是多少,比如输入的电压是稳定的,采集的精度的百分比是多少?不是分辨率
  • 您好,
    当输入电压很低的时候,TLV2553的转换的数字量偏差很小,比如SPI读取的数字量为120时,偏差仅有±3的样子,当数字量变为3500时,其SPI读取的数字量偏差最大能达到±(40~50),不太明白为什么,SPI读取的数字量较小时,偏差比较小,SPI读取的数字量比较大时,偏差就比较大。
    另外,我想确认一下,TLV2553的采集精度是多少,比如输入的电压是稳定的,采集的精度的百分比是多少?不是分辨率