Other Parts Discussed in Thread: ADS1120
你们好,
使用ADS1120测量K型热电偶时遇到一个问题,按照datasheet上的描述,在热电偶输出信号的正负信号分别加2M的上拉和下拉电阻以提供共模电压,
改造完电路便输入MV值来验证ADS1120测量电压的正确性,但是发现ADS1120的电压测量值与输入电压严重不符且有波动,例如输入40mv的电压,
ADS1120的测量值只有10-11mv,我是按照datasheet推荐的电路连接的,也参考了一些参考设计,不知道问题出在什么地方。
ADS1120的配置:
1、AIN2作为AINP,AIN3作为AINN.
2、PGA enable,Gain=32
3、20sps,使用内部2.048V参考电压,持续测量模式。
以上配置已经在PT100以及压力传感器的测量上使用,没有问题,测量电压也比较准确,但是当按照datasheet改造电路后就出现电压值测量不准确的问题,感觉
是ADS1120没有工作正常,不知道问题出在哪里。