This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下关于DS90UB913/953噪声问题



你好,如下有两个疑问,还请帮忙解答:

两款产品分别使用:913配对914,953配对954,线长5米。两种方案,使用同一片sensor。

1. DS90UB913/953电源噪声SPEC中推荐为25mV,实际测量在30mv~45mv,请问是否影响芯片正常长时使用?

2. 913所在的sensor板,在对其机壳打8K气隙静电时,一打就挂。降到2K同样如此。极易受到空气中电磁波干扰。目前定位到是913-914出现了问题。

    但是953-954方案静电测试时并未出现这种情况。PCB布局基本无差异。

    请问下913/953之间,在电源、差分信号、噪声容限、静电实际承受能力等等方面有什么差异,能通过哪种方式确认到具体信号问题。

以上,还请帮忙解惑,感谢

  • DS90UB913/953电源噪声SPEC中推荐为25mV,实际测量在30mv~45mv,请问是否影响芯片正常长时使用?
    我觉得长时间使用, 应该没有问题, 正常使用呢, 可能电源的噪声导致能使用, 但对信号采样的精度受影响
  • 要求电源噪声最大不超过25mVpp。超过这个值的话,不能保证正确通讯,在通讯过程中应该会有一定的误码率。
    2) 关于913和953 二者之间ESD等级的差异,在datasheet中都有给出,ISO/IEC的contact discharge能达到7KV,8KV, air discharge达到15Kv。
    913使用的是913Q还是913A?5m的 cable类型使用的是coaxial还是STP? 如果使用913Q的话只能使用STP。