Dear TI
我司用DT83TC811S-Q1作为车载以太网外部PHY,MAC是MTK的MT2731。我们需要支持MII/RMII/RGMII三种协议。附件是我司做的原理图,请帮忙检查是否有错误。
另外有几个问题
1.芯片pin10(INH)原理图中只外拉了一个测试点,是否可行
2.PIN16(CLKOUT/GPIO_2)原理图中悬空,是否可行,悬空有没有风险点
3.TRD_M&TRD_P与外部连接器之T102_SUB_V1_20200309B.pdf间是否需要网络放大器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI
我司用DT83TC811S-Q1作为车载以太网外部PHY,MAC是MTK的MT2731。我们需要支持MII/RMII/RGMII三种协议。附件是我司做的原理图,请帮忙检查是否有错误。
另外有几个问题
1.芯片pin10(INH)原理图中只外拉了一个测试点,是否可行
2.PIN16(CLKOUT/GPIO_2)原理图中悬空,是否可行,悬空有没有风险点
3.TRD_M&TRD_P与外部连接器之T102_SUB_V1_20200309B.pdf间是否需要网络放大器
1.因为不知道这个信号是不是必须连接,增加测试点是为了预留,方便调试过程飞线。如果确认不需要连接INH信号,那么可以去除测试点。
3.是网络变压器,我们以前做1000Base-T 标准的以太网都会在PHY和RJ45接口之间放一个网络变压器,主要目的为了增加信号的传输距离,如果不加网络变压器数据传输距离就非常短 ,只有几十厘米,线路稍长就会出现断续。现在是1000Base-T1标准的以太网,我们就不清楚需不需要增加网络变压器了。