在使用运放驱动AD时,中间要加一个一阶无源低通电路,其中电容为什么要使用银云母或COG这种类型的电容?而像X7R,Z5U这样有电压频率“记忆”效应的电容,会降低ADC的总谐波失真?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用运放驱动AD时,中间要加一个一阶无源低通电路,其中电容为什么要使用银云母或COG这种类型的电容?而像X7R,Z5U这样有电压频率“记忆”效应的电容,会降低ADC的总谐波失真?
这里有一份有关电容的总结,希望对您有所帮助。在选择SAR ADC 输入充电电容时,理论上应该选择容量随频率、温度、电压变化较小的COG电容。
这个问题的根本原理是这样的,由于像X7R和Z5U这样的电容的容值会随着加在他上面的电压变化而变化。因此这个电容值可表示为C=C0(1+KV)。其中V是加在上面的电压,K就是电容的电压相关系数。由于ADC的输入电压是变化的,如果采用X7R电容,则电容值会随着电压发生变化。这就进一步引起给这个电容充放电的电流也会随着电压发生变化。当这个不稳定的电流流过ADC的输入端时,会在输入端阻抗上形成误差电压。这个随电压变化的电流会使得这个误差电压的随输入电压发生变化。当输入信号是正弦波时,这个误差电压会包含谐波成份。
因此一些资料上,会推荐使用稳定性高的电容,如云母的,或COG的电容。像X7R和Z5U电容,其容值不只与电压有关,还会随频率的变化而变化。可能还会有其他影响斯稳定的因素。
有文献上做了相关仿真。从仿真结果看云母电容和C0G电容,在电压变化和频率变化时,引起的THD恶化最小