大家好!
我最近准备使用ADS1230这款AD,供电电压预计为3.0V(AVDD = DVDD = REFP = +3V),然而手册上找不到3.0V供电时,模拟输入端口支持的共模电压范围的数据,只有5V供电时的数据,即AGND + 1.5V~AVDD – 1.5V,当使用3.0V供电时,显然这个数据是不能直接套用的
想请教各位,是否知道这款芯片工作于AVDD = DVDD = REFP = +3V的时候,模拟输入端口支持的共模电压范围?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您这边使用ADS1230 是否为桥式传感器应用呢?user6539130 说:谢谢您的及时回复!这样的话我的项目就可以开始啦!十分感谢!
嗯是的,因为ADS1230主要是用于桥式传感器的应用,那么传感器的输出正好是激励电源的1/2. 如果是其他应用的话,建议选择其他ADC再看看。user6539130 说:如果是这样的话,我有必要考虑换个ADC了,即便是桥式传感器,因为内部补偿或者调零电路的原因,也不能保证共模电压范围在+-0.5VVref/Gain这个范围内的,TI的ADS1120里的输入共模电压范围的算法应该跟您之前说的很类似,我也有过猜测,如果PGA结构是类似的,那么可以参照您的计算方法,看来是不行了