Other Parts Discussed in Thread: ADS1675, THS4521
我在使用ADS1675时,发现这个ADC很容易受外部的EMI信号而停止采样。
芯片工作在WIDE-BANDWIDTH FILTER模式,开始采样时,我将START信号一直置为1,正常工作时芯片会周期性的输出DRDY(频率为目标采样率)信号,但是一旦受到外部的EMI干扰信号,芯片就不会输出DRDY信号,数据信号为0,这个时候用万用表量START信号,还是保持高电平的。如果不对芯片进行操作,芯片一直保持这种非正常的工作模式。如果人为的将START清零,然后再拉高,芯片可以恢复正常工作,后面再受到EMI干扰信号,还会进入非正常工作模式