This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BP-DAC11001EVM: Hardware not connected

Part Number: BP-DAC11001EVM
Other Parts Discussed in Thread: MSP-EXP432E401Y

Dear sir

i have already mounted the BP-DAC11001EVM evolution board

on the MSP-EXP432E401Y Launchpad,and connect to pc

but the firmware home page show controller is not responding

i check the serial port configuration,the MSP-EXP432E401Y can be detected (see attach)

,it means the  BP-DAC11001EVM evolution board is not responding or MSP-EXP432E401Y ?

could you please give me any help

  thanks!!

      Alex  

  • 您好, 您的问题和E2E上这个问题类似, 试试tab栏中的options-serial port中更换一个其他COM口试试呢:

    e2e.ti.com/.../bp-dac11001evm-bp-dac11001evm

  • Dear sir

    could you please check the USB ,and jumper connect as attach

    furthermore the BP DAC11001EVM must be mounted on the  MSP-EXP432E401Y

    if not do so,Hardware connected may show fail ? right?


    thanks!!

    Best Regrd!!

  • Hello, what about your questions? Your hardware looks like no problem, and it appears "Hardware connected".

  •  Dear sir

    i just want to check the jumper connect is correct or not?Because today i find the hardware is malfunction again

    when the  MSP-EXP432E401Y connect to my pc,there is no response 

     thanks!!

  • Hello, the hardware setup between MSP430 lauchpad  and BP-DAC11001EVM should be as this. It looks different with your setup, which jumper or interface do you use to connect between them?