This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir
i have already mounted the BP-DAC11001EVM evolution board
on the MSP-EXP432E401Y Launchpad,and connect to pc
but the firmware home page show controller is not responding
i check the serial port configuration,the MSP-EXP432E401Y can be detected (see attach)
,it means the BP-DAC11001EVM evolution board is not responding or MSP-EXP432E401Y ?
could you please give me any help
thanks!!
Alex
您好, 您的问题和E2E上这个问题类似, 试试tab栏中的options-serial port中更换一个其他COM口试试呢:
e2e.ti.com/.../bp-dac11001evm-bp-dac11001evm
Hello, what about your questions? Your hardware looks like no problem, and it appears "Hardware connected".
Dear sir
i just want to check the jumper connect is correct or not?Because today i find the hardware is malfunction again
when the MSP-EXP432E401Y connect to my pc,there is no response
thanks!!
Hello, the hardware setup between MSP430 lauchpad and BP-DAC11001EVM should be as this. It looks different with your setup, which jumper or interface do you use to connect between them?