This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60501: DAC60501输出为0的问题

Part Number: DAC60501


选择DAC60501M,采用3.3V供电(VDD),内部REF,按照默认值通过SPI配置寄存器,REF_DIV = 0, BUFF_GAIN = 0输出始终是0

正常midscale默认输出应该是1.25V吧?

查阅别人的问题  “是因为内部REF电压大于0.5*VDD(1.65V), 所以要设置REF_DIV = 1,进行2分频,然后设置2倍输出增益,就可以了。即发送24’h040101设置寄存器4。”

不知道是这样的吗?参考7.3 Recommended Operating Condition有类似说明,但是这是外接REF,内部REF也有类似要求吗:REF要小于0.5*VDD?

非常感谢

  • 您好,是这样的, 7.3 Recommended Operating Condition 针对的不仅仅是外部参考,也适合内部参考.

    datasheet 8.3.2 Internal Reference有介绍,either internal reference from external reference, 都参考7.3推荐的电气参数表格.