This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: 实现十二导数据采集时,导联接触不牢,造成波形上出现锯齿波的问题

Part Number: ADS1298


我参考ADS1298的评估版的连接方式连接各个导联线的位置,如图所示。我在佩戴测试中发现,如果电极贴敷身体牢固可靠的情况下,采集到的心电波形都很正常干净。但当电极片贴敷人体不是很牢固,比如夏天出汗或者电极上的导电凝胶与皮肤不是贴敷很牢固充分时,该导联采集到的数据会出现规律的锯齿波纹状态,而且相邻采样点的数值会规律地一高一低出现,如图所示的现象。此时刻其他电极粘附牢固的导联采集到的波形都正常。我采用的是低功耗模式250的采样率。采用的是电流源直流导联脱落模式检测导联是否脱落,导联脱落比较器正极侧阈值为70%,负极侧阈值为30%,采用固定斩波频率fMOD/16,。各个寄存器的配置如下:
CONFIG1=0x06
CONFIG2=0x32
CONFIG3=0xCC
LOFF=0xE3
CH1SET=0x00
CH2SET=0x00
CH3SET=0x00
CH4SET=0x00
CH5SET=0x00
CH6SET=0x00
RLD_SENSP=0xFF
RLD_SENSN=0xFF
LOFF_SENSP=0xFF
LOFF_SENSN=0xFF
LOFF_FLIP=0x00
LOFF_STATP=0x00
LOFF_STATN=0x00
GPIO=0x0F
PACE=0x01
RESP=0x00
CONFIG4=0x02
WCT1=0x0A
WCT2=0xE3
不知道这样的配置是否是产生这种锯齿波纹的原因呢?我应该如何改进才能不出现呢?谢谢