This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电压放大电路芯片推荐

Other Parts Discussed in Thread: LM358, OPA188, OPA2188

各位,

我现在手上的案子需要有一个电压放大的功能,基本需求是:

单片机的DAC出来的0~2.5V电压,但是需要进行放到到  -10V ~ 10V,能不能推荐一下运放啊?

之前的一个产品我用的LM358来做的0~5V的范围,现在就不知道怎么玩了。:(

能不能给点帮助啊?