Other Parts Discussed in Thread: LM358, OPA188, OPA2188
各位,
我现在手上的案子需要有一个电压放大的功能,基本需求是:
单片机的DAC出来的0~2.5V电压,但是需要进行放到到 -10V ~ 10V,能不能推荐一下运放啊?
之前的一个产品我用的LM358来做的0~5V的范围,现在就不知道怎么玩了。:(
能不能给点帮助啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
附件是TINA仿真,供参考。不过此仿真的输入电压是0.33V-2.97V,楼主只需根据原理分析和数学计算改变电阻的参数即可满足要求。希望能够帮到您!
这个是要看楼主你自己的需求了,如果说你0~2.5V输入,既要得到0~10V输出,也要得到-10~0输出,那你就要搭2个电路,然后根据需要来进行选择使用哪个输出。
如果你就是要把0~2.5V放到到-10~10V的范围(比方说0变到-10V, 2.5变到10V),则可以通过2级来做,前面做个减法运算(Vin-1.25V),后面做个gain=8的放大即可。
嗯,明白你所说的,你能告诉我这两种做法的优缺点吗?从我的需求角度来说,并不需要同时得到0~10V以及-10~0V的电压,你说的第二种方法即可,但是第二种方法因为Gain=8,会不会导致误差会被放大?如果误差并不是线性的话,可能会导致Calibration很麻烦。
另外,如果用你建议的第二种方法的话,选用TI的什么芯片?
这两种方法其实是同一个道理,都是采用加法电路来实现的,如果您需要的-10-0V和0-10V两级输出,那么建议你做两路调理来实现,采用OPA2188即可,双通道放大器。如果需要直接得到-10-10V输出,一级调理电路即可。附件是0.33V-2.97V输入,0-10V输出的仿真电路,希望可以帮到您。