您好,
我正在使用ADS131E08做设计,在使用SPI读取ID以及接受信息的时候,采用低于2M的速率,一切正常,但是当我使用更高速率的时候,比如12MHz, 则寄存器不能正常读,SPI OUT恒为低电平,请问是不是有其他需要设置的地方才能使用高速率。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,2M速率您这里指的是master clock input,还是SPI的SCLK频率?
如果是master input的话,最大频率不超过2.25Mhz。

您好,使用高速率不需要别的设置,只是不同的DVDD电压的SCLK的最大频率不一样,这是在不同DVDD电压范围的SCLK的频率范围,可以看到,当DVDD在1.7~2V之间时,fCLK(max)不超过1/66.6=15MHz. 如果在2.7~3.6V之间时最大频率不超过20Mhz,您的DVDD电压是多少呢? 另外,SCLK的jitter是否很大?DOUT一直为低电平,DRDY时序正常吗?