This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: ADC12DJ3200 1V1供电咨询

Part Number: ADC12DJ3200
Other Parts Discussed in Thread: ADC12DJ5200RF, TPS7A92

手册章节9.1  上电顺序这里 以及上一页的电源连接方式提到A1V1和D1V1 使用建议(而非强制)口吻,要求使用同一个电源芯片供电,这样电压可以保持完全一致。但是根据我们这边的设计经验,模拟/数字电源会互相串扰干扰。一般我们会使用2个LDO分别给A1V1/DAVA供电。这个建议有什么说法,独立供电两种1V1有什么潜在隐患,两个调节器导致的电压差异有什么影响

  • 您好,

    使用同一个电源芯片主要是为了上电时它俩的上电顺序一致,或者说需要同时上电。

    这里也 提到了相互干扰的问题,这里的建议是使用铁氧体磁珠滤波器隔离 VA11 和 VD11 以防止它们相互影响

  • 磁珠铁氧体的隔离效果在我们这边评估隔离效果并不是很好。手册这块只是描述了通过共用电源就不存在电压差异和1.1v之间的上电顺序问题,也就是说两种1v1之间存在上电顺序要求 还是要求不允许压差的问题。现有设计肯定是要分开设计1v1,是否存在较大隐患

  • 我查看了ADC12DJ5200的手册,其手册中P194页对上电顺序也有同样的要求(https://www.ti.com/lit/ds/symlink/adc12dj5200rf.pdf  )

    同时查看了其EVM板原理图,VA11 (开关稳压器+LDO)和 VD11(开关稳压器)使用了不同的供电IC。

    因此,我进一步认为这里主要的问题是在上电期间,两种1V1需要同时上电。如果您需要不同的电源芯片产生这两种1V1,我去确认下,在上电期间这两种1V1可以允许的电压差

  • 我们的设计是同一个DCDC输出1.6V中间电压,然后使用2片TPS7A92  2a LDO分别给va11和da11  理论是同时上电

  • 抱歉,我没有查到上电期间这两种1V1可以允许的电压差;如果这2个LDO能够同时给VA11 和VD11上电,这应该是没问题的