This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS52J90: SYSREF与SYNC信号连接方式

Part Number: ADS52J90


您好,在ADS52J90的手册中,要求SYSREF和SYNC信号在使用LVDS电平的时候,需要使用电平转换。

但是在EVM的原理图中,从LMK到ADC的SYSREF只是使用了交流和100 Ohm端接,从FPGA到ADC的SYNC只是采用了100 Ohm端接,都没有采用电平转换。

设计的时候采用EVM的连接方式,是否会有问题?