Part Number: AFE5401-Q1
参考时钟输入为100MHz,设置4分频,但是DCLK无输出,还需要设置哪边的寄存器或者是管脚
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,输入时钟频率如果是100Mhz的话 ,需要DIV_EN, DIV_FRC enabled,并且Register 01h的DIV_REG = 3.都配置了吗?

SPI 参考的是DVDD,而DVDD 的电压范围为1.7V~1.9V,典型值为1.8V,所以SPI 为1.8V的呢。