This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC34J45: 通过JESD204B与FPGA连接时,出现p/n交叉的情况,是否可以p/n交叉连接(即FPGA的差分线的xx_p连接ADC的dx_m)

Part Number: ADC34J45

您好,下图左侧为FPGA核心板在底板上的接插件,通过JESD204B方式与ADC连接,但布线路径需要交叉。

这种情况应该如何处理?

方案1. 将差分线对内交叉连接,即FPGA的差分线的xx_p连接ADC的dx_m

方案2. 跨层布线。

方案1是否在电气连接上不允许,或者如果可以,是否存在潜在的逻辑问题?

方案2,跨层布线对于3.2GHz的数据速率是否有影响?

或者是否有其他解决方法?谢谢!

x 出现错误。请重试或与管理员联系。