Part Number: ADS1299
在该器件规格书"Table 16 Lead-off Control R...... "项中,配置导联脱落比较器门限寄存器,有几个门限可供选择,即“000:95% 001:92.5%”。我在使用中存在以下疑问:
1.该门限的95%是指多少?是指DAC参考电压的95%吗?DAC的参考电压和ADC使用一个参考源吗?
2.该DAC是一个3位DAC,那边精度应该为1/8=12.5%,但是为什么门限一挡的变化为2.5%呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1299
在该器件规格书"Table 16 Lead-off Control R...... "项中,配置导联脱落比较器门限寄存器,有几个门限可供选择,即“000:95% 001:92.5%”。我在使用中存在以下疑问:
1.该门限的95%是指多少?是指DAC参考电压的95%吗?DAC的参考电压和ADC使用一个参考源吗?
2.该DAC是一个3位DAC,那边精度应该为1/8=12.5%,但是为什么门限一挡的变化为2.5%呢?
您好,
数据手册没有明确给出DAC的参考电压,我在下面链接手册看到了如下示意图,这里的000:95% 001:92.5%应该指的DAC的输出值,是AVDD的百分比。这里DAC怎样输出这8种百分比,我认为不需要我们考虑,它是数据手册告诉我们的,我们直接使用就可以了。
正负电极都脱落时,比较器VINP输入应该是AVDD,另一个比较器VINN的输入应该是AVSS。设置的百分比它是对完全脱落时的电压的百分比。
https://www.ti.com/lit/ds/sbas459k/sbas459k.pdf