This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: 导联脱落比较器阈值问题

Part Number: ADS1299


在该器件规格书"Table 16 Lead-off Control R...... "项中,配置导联脱落比较器门限寄存器,有几个门限可供选择,即“000:95%    001:92.5%”。我在使用中存在以下疑问:

1.该门限的95%是指多少?是指DAC参考电压的95%吗?DAC的参考电压和ADC使用一个参考源吗?

2.该DAC是一个3位DAC,那边精度应该为1/8=12.5%,但是为什么门限一挡的变化为2.5%呢?

  • 补充:经过测试,我们对采集通道输入一个共模电压,以下为试验数据:

    (24倍增益 6nA直流激励,设置不通的门限测试脱落临界值。

    95% 2.23V

    90% 1.98V

    80% 1.5V

    70% 1V

    推算出 Y=5x-2.5V  Y为脱落共模电压阈值(即DAC输出的比较值,x为设置的百分比),那么DAC参考应该是试验的ADC的正负模拟电源(我们用的±2.5V供电)

  • 您好,

    数据手册没有明确给出DAC的参考电压,我在下面链接手册看到了如下示意图,这里的000:95%    001:92.5%应该指的DAC的输出值,是AVDD的百分比。这里DAC怎样输出这8种百分比,我认为不需要我们考虑,它是数据手册告诉我们的,我们直接使用就可以了。

    正负电极都脱落时,比较器VINP输入应该是AVDD,另一个比较器VINN的输入应该是AVSS。设置的百分比它是对完全脱落时的电压的百分比。

    https://www.ti.com/lit/ds/sbas459k/sbas459k.pdf