This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E06: 差分输入RC滤波器对信号幅值的影响,以及测量精度问题咨询。

Part Number: ADS131E06


如图所示是我司使用ADC芯片ADS131E06的差分输入前端电路设计图,输入交流电压或电流信号经互感器(T2T5)转换为mA级别小信号,然后经采样电阻(R8R11)转换为电压信号,R2R14C2C8C5组成共模和差模滤波器。

ADC供电电压:AVDD+2.5VAVSS-2.5VDVDD3.3VADC参考电压为2.5V

目前测试过程中有些问题需要贵方的支持,测试方法及现象描述如下:

1)使用标准信号源给互感器输入一额定电压的工频电压(50HZ)源,每个周波采集40个点,程序计算后的有效值精度超过了1%,且不稳定在飘动(1%~3%);

2)使用精密万用表测量ADC芯片输入端电压(即图中的电容C5两端),测出的电压值与理论计算值偏低(超过1%),若去掉RC滤波器,测出的电压值与理论计算值偏差很小。请问该RC共模/差模滤波器对信号电压幅值的影响原理是什么?是因为我们的3dB截至频率设置过低了嘛?

3)我们准备输入直流信号来进行ADC采样精度及稳定性测试,于是将ADC差分输入INxP接直流信号源输出正极,INxNAGND((AVDD+AVSS/2),并与直流信号源输出负极相连,发现ADC无法测量出直流信号,程序计算出的值完全不对,请问这是为什么呢?

急等,谢谢!