This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A02: 读取数据状态为0x2232,

Part Number: ADS131A02


你好,
1、SPI的时钟频率为2.5MHz, 

2、数据转换器的时钟寄存器配置:CLK1:0x08 , CLK2:0x86

在读取模拟数据时,出现0x2232状态,请问这个怎么解决?

盼复,

谢谢!

  • 您好,能详细描述下您的问题吗?这颗ADC我需要花点儿时间去看下它的数据手册,目前看来是CLK1和CLK2都是默认配置,读取的数据有误,可以读取下状态寄存器0x05h和error count寄存器0x06h,看下是哪里报错。

  • 你好

    这款数据转换器,我采用:
    1、M0 = H, M1 = L, M2 = L,数据24bit, 采用16.384MHz的外部时钟源,故使用synchronous master mode 工作模式;

    2、SPI的时钟源为84M,可做分频调节,现在分频为2.5MHz,CLK1和CLK2都是默认配置,寄存器配置完成后,读取状态寄存器0x05h和error count寄存器0x06h, 分别是0x2501和0x2600, 在此条件下可以正常配置数据转换器的寄存器,并读取到相应的配置值.

    3、在读取ADC数据时,读取的状态为就为0x2232,请问这个问题怎么解的呢

    谢谢

  • 您好,SPI clock的时钟源位84Mhz,超出了datasheet中给出的频率范围呢。IOVDD>2.7V时, SCLK最大频率为25Mhz。小于2.7V时,最大为15.6Mhz。