Part Number: ADS1256EVM-PDK
Other Parts Discussed in Thread: ADS1256, REF6050
本人对ADS1256进行测试和应用,希望得到你们测试ADS1256的测试环境照片以及测试视频(本人不做商业用途),并希望能够给予测试信号源的型号。能够发一份你们在测试ADS1256的测试数据以及测试的MATlab代码,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1256EVM-PDK
Other Parts Discussed in Thread: ADS1256, REF6050
本人对ADS1256进行测试和应用,希望得到你们测试ADS1256的测试环境照片以及测试视频(本人不做商业用途),并希望能够给予测试信号源的型号。能够发一份你们在测试ADS1256的测试数据以及测试的MATlab代码,
您好,
非常抱歉,我们没有针对ADS1256测试的环境照片以及测试视频,也没有测试的MATlab代码,但是我在 TI 高精度实验室 – ADC系列视频 中看到第5章节有ADC的频域指标,像谐波失真,信噪比。以及如何优化和测量频域指标的讲解,希望对您有帮助:
TI 高精度实验室 – ADC系列视频:edu.21ic.com/.../1882
1、不一定,是根据设计要求来决定是否加放大电路;
2、我在E2E英文论坛找到了REF6050 TINA-TI Reference Design,您可以打开,复制REF6050 model到您的仿真文件;
3、这只是放大器电路、ADC电路以及参考源电路的噪声,如果在您的信号链中还存在其他器件,系统的噪声还应加上其他器件的噪声。
您好,1、这个模拟信号源的精度是多少?我认为它的精度误差至少在ADC无法检测到的水平,即至少在1LSB的一半以下。ADS1256的1LSB=2VREF/(PGA(2^23 − 1))。
2、您是说万用表六位半的精度吗?那么这样的话是从0 000 000到1 999 999,表示的是200万个数;而将ADS1256的PGA设置为1的话,2^23=8,388,608=800多万,远远大于200万,因此,六位半的精度不满足要求。
3、一般信号源上会存在噪声,噪声一般在高频段,通过滤波器可以降低噪声,提供信号精度。