Part Number: ADS1148
Hi TI 专家,
1.ADS1148如果使用了外部基准,为啥还要开内部基准,是基于什么考虑开内部基准?
2.偏置电压,打开好还是关闭好,基于什么考虑?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于这个器件,还有问题想向您请教:
1.ADS1148这块芯片,接三线PT1000需要接两路激流源,AIN0-AIN7都可以作为激流源输出吗?如果设置激流源输出1mA,也是可以达到吧。
1、是的,AIN0-AIN7都可以作为激流源输出,可通过IDAC1(地址0Bh)寄存器设置,如下截图:

2、
如果设置激流源输出1mA,也是可以达到吧。
是的,可以设置1mA,最大可以设置到1.5mA,如下寄存器配置说明: