This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J69: Jesd204链路及DDC问题

Part Number: ADS54J69


1、ADS54J69的内部两个转换器A和B输出的采样的数据是通过一个Jesd204b链路(8个lane)还是通过两个独立的jesd204b链路(每条链路4个lane)。

2、ADS54J69有个DA_BUS_REORDER寄存器,手册上该寄存器只有0x0A一个配置选项,请问该寄存器是如何实现通道对应的?

3、ADS54J69每个转换器后跟随两个半带的FIR滤波器,那输出的是IQ数据吗(但内部没有混频器)?如果是的话,那最终jesd204b输出的数据格式是是什么样的呢?

  • 1.  通过Figure 71的架构图可以看到,应该是两个4lane的JESD204B链路。

    2.关于这个寄存器,看起来确实没有详细对这8bit详细介绍,我理解的是A bus或者B bus的recoder是通过配置Table 12中列觉得寄存器来是实现的。

    3. output format可以通过寄存器43h来配置。

  • 1、AD配置为4222模式,reg52配置08,reg72配置为08,按图74所示应该是从lane0和lane1输出数据,但实际确实从lane1、lane2和lane3都有数据输出(lane1和lane3数据相同);如果reg52及reg72都配置为00,则只有lane2和lane3有数据。因此感觉数据与通道对应和手册的不一致。

    2、AD输入采样时钟为500M,采用4222模式,2倍FIR抽取,输入10M单音信号,结果画出的频谱有很多谐波,而且频率越高谐波越多,请问可能是什么原因。

  • 您好,关于您的问题,稍后我这边给您答复。

  • 您好,抱歉回复晚了。

    1)0x52=0x80,0x72=0x80.

    2)谐波很多的话,要确保输入单音信号通过滤波来解决。 如果仍不能解决的话, 可以将配置的寄存器附上,看下寄存器的配置。