1、ADS54J69的内部两个转换器A和B输出的采样的数据是通过一个Jesd204b链路(8个lane)还是通过两个独立的jesd204b链路(每条链路4个lane)。
2、ADS54J69有个DA_BUS_REORDER寄存器,手册上该寄存器只有0x0A一个配置选项,请问该寄存器是如何实现通道对应的?
3、ADS54J69每个转换器后跟随两个半带的FIR滤波器,那输出的是IQ数据吗(但内部没有混频器)?如果是的话,那最终jesd204b输出的数据格式是是什么样的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 通过Figure 71的架构图可以看到,应该是两个4lane的JESD204B链路。

2.关于这个寄存器,看起来确实没有详细对这8bit详细介绍,我理解的是A bus或者B bus的recoder是通过配置Table 12中列觉得寄存器来是实现的。
3. output format可以通过寄存器43h来配置。

您好,抱歉回复晚了。
1)0x52=0x80,0x72=0x80.
2)谐波很多的话,要确保输入单音信号通过滤波来解决。 如果仍不能解决的话, 可以将配置的寄存器附上,看下寄存器的配置。