最近我用到ADS1282开发一款新产品,它是一款31bit的AD,但是我调试后只能做到21,22位的样子(采样速率为250SPS),我的放大倍数为1,不知道是芯片本身只能达到这性能,还是我设计上存有问题??急盼答复,谢谢...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照datasheet:http://www.ti.com.cn/cn/lit/ds/symlink/ads1282.pdf 第十三页的信噪比参数,250SPS采样率 PGA=1时对应的信噪比是130, 按照理想信噪比与有效位的关系 SNR=6.02n+1.76, 有效位可以到达21.3位。
按照31位输出,21位有效位,10位noise,
最小分辨率(设REF=2.048V, PGA=1) , 2.048/[2*(2^30-1)] * (2^11-1) =2uF
10位噪声啊,那为什么还要设计31位的ADC呢?反正低几位都已经是噪声了,24位的岂不已经够用了啊?这样把噪声采回来有什么特殊的用途吗?谢谢!
要是你的信号源只有21位精度,ADC再好也没法给出22位精度啊。所以要想评估ADC本身的噪声,你可以先试试把ADC输入短路,这样采到的值就都是ADC本身的噪声了,如果低8位在跳,那就是低8位是噪声,以此类推吧。
这个我知道,但是上面 Johnsin Tao说1282是31位输出,21位有效位,10位noise,那跟24位的1675岂不是差不多,多的那几位也都是噪声了
ADS1675是个4M,24bit的SDADC。按照手册16页表1,有效位是18~19位。ADS1282是4K,31bit的SDADC,按照手册13页表1,有效位大约是21位。个人观点,这两个ADC不能直接类比,因为速度相差太大。如果短路输入,仍然是低10位在跳,那就可以确定低10位是噪声了,否则有理由怀疑信号源不干净。
24位的,计算出来有效位大约在16位左右,也会存在8位的噪声。因此噪声位是一定会存在的,不是说只是31位的ADC才存在噪声位。