This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: 波形输出异常,请帮忙分析问题点,确定一下调试思路

Part Number: ADC12DJ3200


测试1adc12dj3200的通道1的输入800mV,无论单通道还是双通道,fpga的数据中偶数路波形看着正常,奇数路波形不对。通道2输入,波形都正常。

改到200mV后波形如下:

测试2:将adc配置为测试模式,0x205寄存器配置为04.

通道1的波形如下:

 

 

通道2的波形:

 

对比发现,通道2s0s1是一样的,s2s3是一样的,s4s5是一样的,s6s7是一样的,s8s9是一样的。

通道1的不是这样。这个现象和接入输入信号是一致的。

 问题:请帮忙分析问题点,确定一下调试思路