Part Number: ADS1263
ADS1263配置为速率50SPS,周期DELAY_35us,单端测试,基准选择为外部供电电压(AVDD-5V,AVSS),增益分别设置为1,2,4,8,16,32。用干电池进行测试,干电池电压为1.5V,增益1,2,4,8,16,32测试的结果分别为:
1.51V,2.01V, 2.45V, 2.65V, 2.90V, 2.99V。其测试结果不是线性的。请问这个是什么原因引起的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1263
ADS1263配置为速率50SPS,周期DELAY_35us,单端测试,基准选择为外部供电电压(AVDD-5V,AVSS),增益分别设置为1,2,4,8,16,32。用干电池进行测试,干电池电压为1.5V,增益1,2,4,8,16,32测试的结果分别为:
1.51V,2.01V, 2.45V, 2.65V, 2.90V, 2.99V。其测试结果不是线性的。请问这个是什么原因引起的。
不管单端输入还是差分输入都需满足方程式12,单电源供电的话,即 VINP和VINN最小值需大于0.3V,单端输入的话,VINN接的是什么?接地的话是不满足的;
您对PGA是否线性工作这里还存在疑问吗?