This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: PGA放大不是线性的

Part Number: ADS1263


ADS1263配置为速率50SPS,周期DELAY_35us,单端测试,基准选择为外部供电电压(AVDD-5V,AVSS),增益分别设置为1,2,4,8,16,32。用干电池进行测试,干电池电压为1.5V,增益1,2,4,8,16,32测试的结果分别为:

1.51V,2.01V, 2.45V, 2.65V, 2.90V, 2.99V。其测试结果不是线性的。请问这个是什么原因引起的。

  • 您好,

    模拟电压AVDD您是使用单电源5V供电是吗?基准电压是5V?如果是这样的话,在PGA设置为4及以上值时,输入干电池电压1.5V就不满足ADC的输入电压范围了,因为在PGA=4时,基准电压VREF=5V,差分输入范围是±5/PGA,即正电压小于1.25V;

    另外,在使能PGA时,VINP和VINN 的绝对输入范围需满足方程式12,即如下截图,VINP和VINN最小值需大于0.3V

    最后,您是否确认了寄存器写入后可以正确读出?也就是PGA寄存器是否按期望值配置进去

  • 但是设置为2的时候,理论上就应该是3.0V。后来改为差分输入,内部+-2.5V为基准,PGA线性则正常。谢谢解答。

  • 不管单端输入还是差分输入都需满足方程式12,单电源供电的话,即 VINP和VINN最小值需大于0.3V,单端输入的话,VINN接的是什么?接地的话是不满足的;

    您对PGA是否线性工作这里还存在疑问吗?

  • 是的,单端 VINN接地是不行的,单端不能线性放大问题就是出在这,差分可以接地。谢谢!