大家好!
我在使用ADS8668来进行信号采样时发现一个问题,AD接入电路后将导致运放输出端存在100mV的直流量,经过运放放大几十倍后在运放输出端就变成了4V左右的直流量,严重影响后级电路的工作,使用隔直电容也只能减轻这种影响但不能完全消除。
不知道为什么会存在这个问题。是否需要在采样通道串联一个电容来隔直?但这样也只能采样到交流信号,会丢失掉直流电压信息了。
以下是相关的电路


谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
断开SIN_X_3之前的隔直电容,且断开SIN_X_4之后的隔直电容,这样相当于运放没有有效输入信号,若将SIN_X_3连接至ADS8668,那么我想可能是ADS8668内部的PGA电路对SIN_X_3节点电压产生了影响。如下ADS8668内部电路与SIN_X_3的连接情况,PGA的同向输入端有个VBx的电阻分压,PGA反向输入端与其同向输入端电压相等(根据虚短),那么AIN_xP可能会存在一个电压引入SIN_X_3节点,并对其造成影响。
您是否有办法对SIN_X_3加一级电压跟随然后再接入ADC的模拟输入端?看SIN_X_3上是否还出现100mV的直流电平?我想通过电压跟随器来隔离ADC对SIN_X_3节点的影响,来验证上述猜测。