This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这边采用ADS1255作为数据采集,由于芯片描述内部有buffer且输入阻抗为80M,因此输入信号未在外部加buffer,然后发现输入信号采用2个5M电阻分压测试电压不准,撤掉输入信号后用外部万用表直接测量AINCOM和AIN1之间电压,发现有1.2V左右的浮电(考虑万用表输入阻抗10M欧,这个浮电带载能力比较强)。 芯片配置为STATUS=0x02(使用buffer),MUX=0x18(AIN1为+,AINCOM为-),ADCON=0x00(放大倍数1),采样率采用5/100SPS均有浮电。AINCOM接地,AIN1原电路为输入信号采用2个5M分压,AIN1和AINCOM之间的RC滤波去掉和不去掉均有浮电。请问这个浮电是怎么来的,另外对于单端输入超过5V的信号,是否不能直接采用外部高阻值电阻分压后直接输入给AIN1而必须用外部高精度运放做buffer处理后输入?
您好,
这个输入阻抗是指的差分输入阻抗,80MΩ是指在 fCLKIN = 7.68MHz,数据速率是在≤ 50SPS情况下的值。
您是否验证了寄存器写入后可以正确读出来?我想确认下您的寄存器值已正确配置进去;
您可以附上您测量输入端有浮电时的电路图吗?特别是模拟输入端处的电路;
另外对于单端输入超过5V的信号,是否不能直接采用外部高阻值电阻分压后直接输入给AIN1而必须用外部高精度运放做buffer处理后输入?
输入超过5V的话,一个是ADC在buffer on时不满足模拟信号输入范围,buffer on时输入范围到 AVDD − 2.0V,另一个是输入阻抗低,如果信号源阻抗比较高的话,输入至ADC的模拟信号幅值会衰减。
您是在悬空AIN1和AINCOM管脚时测量其差分电压存在1.2V电压是吗?我想这样测量是没有意义的,模拟输入管脚在没有输入时测量其电压相当于测量的外界电磁干扰耦合进的电压。
连接上R16和R19,AIN接采样电压,ADC输出结果也是偏差很大,AIN的电压对ADC值影响很小,主要是浮电电压起主要作用。
我认为这里ADC输出结果偏差很大是因为模拟输入信号的内阻太大的缘故造成的,ADC若使用的数据速率比较大的话,其差分输入阻抗是很小的,在默认30KSPS时是10MΩ,因此测量会存在很大的偏差。
但是我外部加1V或者2.5V,测量结果仍在1.2V这就有问题了
您的意思是说,在连接R16和R19时,AIN不管是接采样电压1V还是2.5V,在电容C30两端测量的电压都是1.2V吗?如果是这样的话,检查下AIN1和AINCOM管脚是否还连接了其他地方?