This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3663: 50M 采样率下 DDC 在Bypass时输出的时钟FCLK占空比不为50%

Part Number: ADC3663


将ADC3663进行50MHz采样,设置如下:2wire、16bits、同时DDC设置为bypass;CLK输入时钟为50MHz、DCLK输入时钟为200MHz,最终测试出的AD输出的FCLK时钟不是25MHz且其占空不为50%的时钟信号,后进行其他采样率测试只要DDC使用bypass,发现AD的FCLK输出均不为占空比50%的时钟信号,而在DDC的抽取率设置为2或其他均正常,请问什么寄存器设置错误可能造成该现象?

  • 您好,

    您可以附上您的寄存器配置吗?同时可以附上您输入和ADC输出的时钟波形吗?

  • 您好,问题已经解决,主要是寄存器设置不正确造成的。
    在不抽取的情况下,需要禁止DDC功能,即需要将0x24寄存器中的DDC使能设置为0。
    我现在有一个疑惑:在不抽取时,0x24 DDC的使能或禁止 和 0x25寄存器中的pypass模式有什么区别,为什么直接采用bypass模式不正确,而采用禁止DDC能够正常输出?