This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1118EVM: 实际监测电压值和输入电压值不符合

Part Number: ADS1118EVM


大家好,

    我运用了这个EVM demo板,之前测试输入电压值,比如在AIN0和GND之间输入1V直流电压,可以通过GUI 看到是一条1V 横线,(显示volts),但是今天再测量1V 的时候,发现GUI显示的电压值在1V上下浮动,我测试了4个端口都是这样,为什么会出现这样的情况呢?

我选择的量程是+/-6.144V,4V 和2V 的量程我也试过,都是一样的结果,然后那个引脚配置,我也配置了AIN0和GND,或者AIN1和GND,都是一样的。