Part Number: TPL0401A-10
如图,我使用TPL0401A-10芯片输出的电阻比值,作为LDO芯片的FB端的分压电阻,RHW/RWL=2.76,FB端的电压为0.8V,这样LDO输出为3V;主机给过来的IIC信号,发现没有应答位,是该线路配置不正确还是可能其他什么问题导致没有应答位的?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPL0401A-10
如图,我使用TPL0401A-10芯片输出的电阻比值,作为LDO芯片的FB端的分压电阻,RHW/RWL=2.76,FB端的电压为0.8V,这样LDO输出为3V;主机给过来的IIC信号,发现没有应答位,是该线路配置不正确还是可能其他什么问题导致没有应答位的?

很高兴问题已经得到解决;
1、很抱歉这里对您造成困惑,这里写的确实不清楚。TPL0401有2种地址,一个是010 1110,一个是011 1110,其中bit5可以是0和1,您所附图片箭头处下划线其实是bit5,因为bit5可以是0和1,所以用下划线代替了。

2、是的,这里是错的,感谢指出。
建议您看最新版的数据手册,B版本:https://www.ti.com/lit/ds/symlink/tpl0401a-10.pdf
您看的数据手册应该是中文版的A版本,中文版的没有更新的B版本: