This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A02: 0-50的温度范围内,ADC输出漂移0.1%

Part Number: ADS131A02


请问ADS131A02在使用中,增益设置默认,当ADC输入3V时,在0℃-50℃范围内,MCU读取到ADS131输出漂移3mV左右;当输入是0.3V时,漂移量则为0.3mV,请问这个现象的如何解释?符合规格书要求吗?