This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: 关于ADS1299芯片的内部参考信号存在的问题

Part Number: ADS1299


工程师您好,我现在正在使用ADS1299一个开发EEG采集系统。芯片的输入电压为+/-2.5V(AVDD=+2.5V, AVSS=-2.5V)

目前将CHnSET设置为测试信号。方波信号的值分别为+1.36mV和-2.37mV,而不是标准的+1.875和-1.875mv。将config2里面的CAL_FREQ[1:0]设置为11变成直流模式,测试的幅值为-2.37mv。

再将CHnSET的MUXn[2:0]设置为001输入短接测试内部噪声,测的噪声值为-0.5mV

目前测试过芯片的参考电压和Vcap电压,Vrefp为+4.499V(相对于AVSS-2.5V)。Vcap1 = +1.198V(相对于AVSS)、Vcap2 = +2.501V相对于AVSS)、Vcap3 = +6.88V(相对于AVSS)和Vcap4 = +2.24V(相对于AVSS)

想问一下如何解决内部测试信号的漂移问题。谢谢

  • 您好,

    PGA的增益您设置的是多少?datasheet中给出的offset是参考输入端的,0.5mV/Gain才是输入端的offset。

    offset典型值是60uV,计算下您的offset  (0.5mV/Gain)是多少?看下是否在spec范围内?