上述高亮的4个指标不太理解
1.Zero-code (negative full scale) error这个是指码值为0时的输出偏差吗?为什么要强调AVSS满量程呢?
2.Full-scale error这个指标的Full Scale指的是40V吗(单极性0到40V或双极性±20V),如果40V范围的的误差是±0.06%,那么±10V的误差是±0.015%吗?
3.Gain Error的单位是%FSR,这也是至40V满量程的误差吗 如果是±10V输出 误差是±0.015%吗?
4.Bipolar-zero (midscale) error 这是指标是指双极性输出时的输出为0V时的误差指标吗 ±0.03%FSR是指40V量程时候的误差吗?
如果±10V输出 这个指标是±0.0075%吗?设定为0V时输出的范围时±0.0075% x 20 = ±0.0015V
我的精度需求是±11V误差优于±5mV,请问使用DAC81402可以实现吗